REGEN.TESTSTATUS

Description

Returns the current status of the regen self-test. See REGEN.TEST for more info about the self-test procedure.

Name

Value

Description

Not Started

0

Test has not been started

Running

1

Test is currently running and has not yet failed

Success

2

Test finished successfully

Timed Out

3

Test did not reach setpoint before timeout configured

Short Circuit

4

A short circuit (fault [2013]) was encountered during the test

Versions

Action

Version

Notes

Implemented

02-07-03-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

REGEN.TEST, REGEN.TESTTO, REGEN.TESTVTHRESH
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
REGEN.TESTSTATUS

3007h

08h

Unsigned8

-

-

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REGEN.TESTSTATUS

2407

967

Unsigned8

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.TESTSTATUS

2407

Unsigned8

Read Only

-